EEO#.POUT

Description

EEO#.POUT is used in conjunction with EEO#.PIN to set the gain of the EEO position going to the EEO Generator. The maximum value of EEO#.PIN / EEO#.POUT is 32.

Versions

Action Version Notes
Implemented 02-07-00-000

General Information

Type Read/Write
Description Sets the gear OUT of the EEO postision
Units N/A
Range 1 to 4,294,967,295
Default Value 1
Data Type Integer
See Also EEO#.PIN
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

EEO1.POUT

4600h

09h

Unsigned32

-

-

Read/Write

No

EEO2.POUT

4601h

09h

Unsigned32

-

-

Read/Write

No

EEO3.POUT

4603h

09h

Unsigned32

-

-

Read/Write

No

EEO4.POUT

4606h

09h

Unsigned32

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

32050

1

32050 (0x7d32)

EEO1.POUT

Unsigned32

Read/Write

Yes

32051

1

32051 (0x7d33)

EEO2.POUT

Unsigned32

Read/Write

Yes

32052

1

32052 (0x7d34)

EEO3.POUT

Unsigned32

Read/Write

Yes

32053

1

32053 (0x7d35)

EEO4.POUT

Unsigned32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

EEO1.POUT

32050

Unsigned32

Read/Write

-

EEO2.POUT

32051

Unsigned32

Read/Write

-

EEO3.POUT

32052

Unsigned32

Read/Write

-

EEO4.POUT

32053

Unsigned32

Read/Write

-